Products:
Topics:
Downloads:
Friends:
Contact Us


Movie Downloads
These are large movie files. Right-clicking and using "Save as" is a good way to save these files to your desktop for viewing.

  • Mideast Checkpoint Firefight Characters driven by DI-Guy AI control a checkpoint when a firefight breaks out. Good example of AI, soldiers, mideast characters, munitions, and DI-Guy Special Effects.

  • DI-Guy AI in action See a city get populated using the DI-Guy AI tool. An excellent video overview of DI-Guy AI capabilities.

  • Avatars An Air Force General gives a presentation. Good example of range of DI-Guy Western civilians and DI-Guy expressive faces. Entire performance was generated from a .wav file of the speech and some photographs of the General.

  • Aircraft Carrier Flight Crew The flight crew prepares a jet for takeoff. Good example of DI-Guy Flight Deck Crew characters and use of DI-Guy Scenario to create a detailed human performance.

  • Policemen discussion Policemen discuss a bomb threat at a conference. Used as a cinematic before the avatar action started. Good example of DI-Guy Expressive Faces.

  • Marines in Baghdad Close up of a DI-Guy Marine.

 

DI-Guy SDK | DI-Guy Scenario | DI-Guy AI | DI-Guy Motion Editor
About DI-Guy | Contact | Home

©2007 Boston Dynamics