SandFlea

About SandFlea


Sand Flea is a small robot with 4 wheels and a mighty jumping leg.  It drives like an RC car on flat terrain, but can jump 10 m into the air to jump over obstacles. That is high enough to jump over a compound wall, onto the roof of a house, up a set of stairs or into a second story window.

The robot uses its wheels as gyros to stay level during flight so the operator gets a clear view from the on-board camera and to ensure a smooth 4-wheel landing. Sand Flea can jump about 25 times on one charge. Boston Dynamics developed Sand Flea with funding from the US Army’s Rapid Equipping Force (REF), DARPA and Sandia National Laboratory.

SandFlea is currently out of production.